您选择的产品已被添加至购物车

S-Polarization

The linear polarization state which is perpendicular to the plane of incidence.  The plane of incidence is normal to the surface or interface upon which light is incident.  If the light is incident upon the interface at an angle, the light will be oscillating in such a way as to appear to be “skipping” across the surface.

See also Polarization , Linear Polarizer , Wire Grid Polarizer , Polarizing Beamsplitter , P-Polarization

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号