The linear polarization state which is parallel to the plane of incidence. The plane of incidence is normal to the surface or interface upon which light is incident. If the light is incident upon the interface at an angle, the light will be oscillating in such a way as to appear to be “plunging” into the surface.
See also Polarization , Linear Polarizer , Wire Grid Polarizer , S-Polarization , Polarizing Beamsplitter
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2025, 爱特蒙特光学(深圳)有限公司 粤ICP备2021068591号
The FUTURE Depends On Optics®