A property arising from the wave nature of light. Polarized light consists of waves which oscillate in a defined and predictable manner. The direction in which the electric field vector points as it propagates through space defines the polarization state. If it oscillates in a single plane, the polarization state is linear. If it rotates about the axis of propagation, the polarization state is elliptical or circular.
See also Polarizing Efficiency , Linear Polarizer , Unpolarized , Wire Grid Polarizer , S-Polarization , Circular Polarizer , P-Polarization , Extinction Ratio , Non-Polarizing Beamsplitter
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2025, 爱特蒙特光学(深圳)有限公司 粤ICP备2021068591号
The FUTURE Depends On Optics®