您选择的产品已被添加至购物车

Surface Accuracy

An indication of the peak-to-valley flatness of a surface given in terms of waves (a multiple or part of a reference wavelength). For example, a specification of 1/4 wave means that the flatness of the surface deviates by one quarter of the wavelength used to test the surface. If the wavelength was 550nm, the flatness would be held to within 140nm in order to produce a surface accuracy of 1/4 wave.  Also given in RMS (root mean squared)  where the peak-to-valley values are squared and then the square root is taken of their mean.

See also Reference Wavelength

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号
;