您选择的产品已被添加至购物车

Retarder (Waveplate)

A class of materials that exhibit the characteristic of birefringence. Orthogonal components of light that enter a retarder (or waveplate) will experience a relative phase shift upon output. This phase shift is dependent upon the thickness of the retarding medium and the degree of birefringence. The axes of the material exhibit different index characteristics and are generally referred to as the fast (low index) and slow (high index) axes.

See also Circular Polarizer , Retardance

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号