您选择的产品已被添加至购物车

Penta Prism

A five-sided prism that deviates the ray path by 90°. Since incident light rays are reflected twice to achieve a right angle turn, the image from a penta prism is of the same orientation as the object. It is useful for shortening the length of an assembly.

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号
;