您选择的产品已被添加至购物车

Optical Density (OD)

Describes the amount of energy that can pass through an optical material. It is directly related to the transmittance of the material, which is the ability of light to propagate through a given medium. A large OD means more blocking.

See also Continuously Variable Apodizing Filter , Blocking , Neutral Density Filter (ND)

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号