您选择的产品已被添加至购物车

What is an ND Filter?

An ND, or neutral density filter, is a type of filter designed to decrease the intensity of the input light without affecting the color (or spectral) distribution. Due to this neutral characteristic, the filters appear gray in color. ND filters are typically designated by their optical density (OD). Transmission for an ND filter can be calculated by using the equation T=10-OD x 100 = Percent transmission Where OD is the optical density of the ND filter. Typical applications for ND filters include decreasing light consistently over the visible or near infrared spectrum, protecting sensing devices from excessive intensity, such as blooming/overexposure of CCD cameras or testing the linearity of a photodetector or photodiode. ND filters are preferred over polarizers for reducing light in the case of extreme light intensities.

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号
;