您选择的产品已被添加至购物车

Is there a limit to the range of angles in which a CGH can be used?

A CGH has a minimum feature size in its interference pattern that limits the maximum possible diffraction angle. This is why an aspheric CGH is often used along with a reference sphere in the interferometer to reduce the required diffraction angles.

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号