Optical Microscopy Application: Brightfield Illumination
Edmund Optics Inc.

Optical Microscopy Application: Brightfield Illumination

作者: Stephan Briggs

Brightfield illumination, which yields dark objects on a bright background, is the simplest technique for optical microscopy. In brightfield illumination, the light source is positioned below the sample. Light then propagates through the sample, and is observed by the objective lens and sensor, which are positioned above the sample. The darker the sample, the denser the specimen, as denser samples absorb more light. The simplicity of brightfield illumination is the main reason this technique is so popular in optical microscopy.

Image Appearance

A typical brightfield illumination image has a dark sample with a white background. The darker the regions on a sample, the more absorption of light that has occurred. For example, plant cells would appear darkest at the nucleus and central region where cellular matter is most dense, and lighter in the cytoplasm void of ribosomes, the endoplasmic reticulum, and other intracellular components. Animal cells are more difficult to image with this technique without staining of the sample, which ultimately kills live cells.

Brightfield Illumination Image of Tissue Paper
Figure 1: Brightfield Illumination Image of Tissue Paper

Technical Details

There are four key components in the light path for brightfield illumination.

  1. Light Source: trans-illumination below sample that propagates through to condenser and objective lens. Typically a broadband source such as a quartz halogen bulb.
  2. Condenser Lens: collects trans-illuminated light and focuses to sample.
  3. Objective Lens: collects light which propagates through sample and enhances details by a factor of magnification.
  4. Eyepiece/Camera: views or records the image.

There are some limitations to the brightfield illumination technique, which include very low contrast for cellular or biological samples, low optical resolution due to limitations of light, and the requirement for stained samples prior to imaging or viewing. However, simplicity of the brightfield technique is a huge benefit when first imaging an unknown sample. Additional optical microscopy applications include darkfield illumination, phase contrast, fluorescence, and differential interference contrast.

本内容对您是否有用?

相关产品

 

 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号