您选择的产品已被添加至购物车

Moment Load

The forces that are offset (cantilevered) from the bearing centers of mechanical components producing uneven loading on the bearings. Uneven loading means that some bearings are supporting more of the load than others. Moment forces are categorized by the direction in which they act: pitch, roll or yaw. When loading results in moments acting in only one of the moment directions, it is called a single direction moment. If it is in more than one direction, it is referred to as compound moment loading.

See also Normal Load Capacity , Yaw , Roll , Pitch

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号
;