您选择的产品已被添加至购物车

Electronic Shutter

Controls the amount of time a camera collects light or charge during each frame, also known as the exposure time. Standard signal formats employ approximately 60 frames per second (fps), indicating a collecting charge of 1/60 seconds for each frame. As light levels increase the sensor overfills with charge, resulting in blooming or streaking. Electronic shuttering circuits prevent these effects by allowing the sensor to collect charge for a shorter period during each frame.

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号
;