您选择的产品已被添加至购物车

Cathode Ray Tube

Video display based on vacuum tube with electron gun and annular anodes at one end and a cathode and phosphor screen at the other. Charged plates or electromagnets deflect the electron beam such that the image is scanned line by line across the face of the tube. Signal response is nonlinear with input, gamma usually between 2 and 3. 

See also Oscilloscope

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号