The future of medical treatment depends on optics-based, non-invasive diagnostics, especially for the treatment of severe burns.
Edmund Optics® (EO) off-the-shelf optics and optomechanics were perfect for SpectralMD’s application requirements. Edmund Optics’ design support, including the detailed CAD files that enabled the design of custom optics by SpectralMD, made it possible to have an excellent collaborative relationship between the two companies. Since, however, SpectralMD was a startup company, they decided to leverage Edmund Optics’ StartUP program to get an extra 10% discount and the dedicated technical support that comes along with the program. Our dedicated StartUP representatives were able to assist them in manufacturing custom optics, modifying stock optics, coring/dicing, and assuring that the quality of optics met their specifications.
From 2018-2019, SpectralMD grew significantly, and once they moved to volume production, they were able to leverage the volume discount that Edmund Optics provides (which often reaches ~20%), instead of the StartUP discount of 10%. Since their growth led to an increase in their technical expertise, and they no longer needed the discount, they graduated from Edmund Optics’ StartUP program.
In 2019, SpectralMD received an FDA breakthrough device designation and have secured a four-year grant made possible by the products and services provided by Edmund Optics. They will be much missed as a StartUP member, and the StartUP team looks forward to seeing them succeed with the help of Edmund Optics’ managed team!
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2025, 爱特蒙特光学(深圳)有限公司 粤ICP备2021068591号
The FUTURE Depends On Optics®