您选择的产品已被添加至购物车
How to Power USB and GigE Cameras: Choosing the Right Accessories

How to Power USB and GigE Cameras: Choosing the Right Accessories

作者: Gianna Riviello

Optimizing your imaging system means more than just choosing the right camera. Selecting the correct camera accessories ensures optimum performance, system stability, and successful integration. This application note explains power requirements for the two most common camera interfaces, USB and GigE, details the essential and optional accessories that enable reliable power delivery, and gives expert tips for selecting the most suitable components for your imaging system.

Understanding Power Options for USB and GigE Camera Interfaces

Choosing between the two main types of camera interfaces, Universal Serial Bus (USB) and Gigabit Ethernet (GigE), depends on several key factors including data transfer speed, system complexity and scalability, cost, and the physical distance between the camera and host PC. GigE cameras provide longer cable lengths and faster transfer rates compared to USB, while USB cameras offer a simpler “plug and play” setup with lower upfront costs. GigE can typically support Power-over-Ethernet (PoE) capability, meaning power and data transfer occur via ethernet using the same cable, with various configuration options. More detailed information on the advantages and disadvantages of each interface can be found in our Digital Camera Interfaces Guide. Powering your GigE or USB camera properly ensures that the system will function as intended. Below, different accessories for powering and optimizing camera setups are discussed.

Powering a USB Camera

The USB Cable

Setting up a USB camera is straightforward—it only requires a USB cable that connects the camera to the computer’s USB port (Figure 1). This cable supplies power to the camera and transmits data to the computer.

Figure 1: Typical USB Camera Setup

Most computers are equipped with USB Type-A ports, which serve as the host-side connection. The type of USB connector on the camera—typically listed in its specifications—determines which cable is needed. A short overview of the USB connectors commonly available is given in Figure 2.

Figure 2: Overview of Common USB Connector Types

Always refer to the camera’s documentation to confirm the connector type before selecting a cable. For example, a camera with a USB Type-C connector will require a Type-A to Type-C cable, while one with a USB Micro-B would need a Type-A to Micro-B cable. When it comes to USB generations, the oldest generation defines the speed of the system. Therefore, it is best to match the generations when possible—e.g. using a USB 3.1 cable with a USB 3.1 camera. Although USB 2.0, 3.0, and 3.1 are backward compatible, data will transfer at the lower supported speed.

The USB Hub Port

In addition to limited cable length of only a few meters, the other limitation of USB is bandwidth. This means that, although multiple cameras can be connected to a PC using a USB Hub Port, they all would share the PC’s bandwidth. Figure 3 below shows a basic setup, where items in green are typically included with the hub port.

Figure 3: Typical USB Hub Port Setup

Powering a GigE Camera (PoE or Non-PoE)

GigE cameras connect to a PC via ethernet. Unlike USB cables, ethernet cables can extend up to 100m and offer more flexible camera positioning. To ensure compatibility, the ethernet cable’s connector typically needs to match the camera’s connector. Commonly used connector types are RJ45 or M12 X-coded. The M12 connector is more robust and often used in harsh environments. It features a threaded locking option to withstand vibrations and offers better protection against dust and moisture. Widely used cable types for GigE cameras are Cat5e or Cat6. Cat5e is limited to smaller distances and cameras with 1Gbps. Longer distances as well as high resolutions and frame rates involve the use of Cat6. Most GigE camera setups require additional accessories beyond the ethernet cable. The following sections outline the available options.

GigE PoE Cameras

The PoE Port Injector

When running a single GigE camera with Power-over-Ethernet (PoE), a PoE port injector would be a simple and easy option to set up the system and provide power and data transfer through the same cable. The port injector has two ethernet ports: one camera connection port for connecting the injector to the camera, and one PC connection port connecting the injector to the PC. To complete the setup, two ethernet cables would need to be purchased. If not included with the device, the port injector requires its own power supply. No additional power source is needed for the camera, which can be a huge benefit in space-constrained applications. A typical PoE injector setup is shown in Figure 4. The port injector is the best option for lower cost, small footprint, and single camera systems.

Figure 4: Typical Port Injector Setup
The PoE Network Switch

When running multiple GigE cameras or even other ethernet devices, the PoE network switch allows for connecting multiple units on a local computer’s network. This setup maximizes available bandwidth per camera in multi-camera orientations. Each camera connects to the switch via a selected ethernet cable used for power and data transfer. An ethernet cable also runs from the computer to the switch. Just like the PoE port injector, the switch would also require its own external power supply if not already included. Figure 5 below shows a typical setup. While a PoE switch enables simultaneous multi-camera connectivity, keep in mind that limited network bandwidth can impact frame rates when many high-resolution or high-frame-rate cameras are connected.

Figure 5: Typical Network Switch Setup
The Network Interface Card (NIC)

The Network Interface Card (NIC) connects to the Peripheral Component Interconnect Express (PCIe) slot of a PC to enhance the network performance of a PC. Similar to the network switch, it typically requires a separate power supply if not already included with the item, and ethernet cables would connect multiple GigE cameras to the card and are used for powering the camera and for data transfer. Up to 4 cameras can be connected to a PCIe card at once. Figure 6 shows a typical network interface card setup. Installing a card requires physically opening a PC to locate its PCIe slot, therefore it is important to understand if there are existing space constraints with a PC before purchasing.

Figure 6: Typical PCIe Network Interface Card Setup

If the selected camera is 2.5, 5, or 10GigE, or requires PoE+, be sure to choose a network interface card that matches the corresponding speed and supports PoE+ functionality. These cards are specifically designed to handle the higher bandwidths and power requirements of high-performance cameras and would be the most optimal way to power your camera.

GigE Non-PoE Cameras

The GPIO

While GigE cameras are often powered using Power-over-Ethernet (PoE), they offer another option for providing power through the General-Purpose Input/Output (GPIO) connector, sometimes also referred to as an I/O connector. For cameras without PoE functionality, the GPIO port serves as the primary power input. In this configuration, power is supplied by an external power supply, not through the ethernet cable. This is ideal for systems where space is limited and efficient power usage with minimal heat generation and low cable transmission losses are essential. The setup would still require the ethernet cable for data transfer, but no PoE device, such as a port injector, is needed (see Figure 7 below). If you are using external devices like trigger hardware, they are also typically connected via the GPIO port. If such hardware is used, the GPIO connector may no longer be available for supplying power to the camera. In this case, the power has to be supplied via a PoE port injector or a cable with flying leads should be considered to provide both power and the trigger signal through separate leads. Hardware options are listed under the “Specifications” tab for each camera if available.

Figure 7: Typical GPIO Setup

Overview of Power Accessories for USB and GigE Cameras

Table 1 provides a quick summary of the power accessories mentioned in the text above. It highlights the products and options you can use for your imaging systems and also gives some basic information to facilitate your decision.

Difficulty of Assembly Cost Number of Devices Supported
USB Cable Easy—Plug and play, provides power and data transfer Low 1
GigE Port Injector Easy—Plug and play with additional wall powered component Low 1
GigE Network Switch Medium—Requires network setup and cabling Medium 4+
GigE PCIe Card Hard—Requires opening PC case and installing card and drivers High 1-4
GPIO Power Supply Easy—Plug into wall power, data cable required Low 1
Table 1:  Overview of Power Accessories

References

  1. Teledyne Vision Solutions. (2015, May 4). Machine Vision Interface Comparison and Evolution: Getting the most out of Integrated Imaging Solution’s USB 3.1 cameras [White paper]. Teledyne Vision Solutions. https://www.teledynevisionsolutions.com/support/support-center/whitepaper/iis/machine-vision-interface-comparison-and-evolution/
  2. Edmund Optics Inc. Camera Types and Interfaces for Machine Vision Applications. In Imaging Resource Guide: Cameras, Section 10.1. Edmund Optics. https://www.edmundoptics.com/knowledge-center/application-notes/imaging/camera-types-and-interfaces-for-machine-vision-applications/
  3. OnLogic. What is PoE (Power over Ethernet)? OnLogic Blog. https://www.onlogic.com/blog/what-is-poe-power-over-ethernet/
  4. LUCID Vision Labs. (Aug 29, 2024). Powering a Machine Vision Camera [Video]. YouTube. https://www.youtube.com/watch?v=CKMWnZZWHbI

More Resources

本内容对您是否有用?

 

 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号
;