您选择的产品已被添加至购物车

Edmund Optics® Simplifies Waveplate Sourcing with One of the Industry’s Broadest Off-the-Shelf Portfolios

Comprehensive selection of waveplates with a wide range of specifications for laser, imaging, semiconductor, quantum, and life science applications.

8/5/2026, Barrington, NJ USA —

Edmund Optics®, a leading global provider of optical and imaging technology solutions, offers one of the industry's broadest off-the-shelf portfolios of waveplates, providing engineers and system designers simplified access to a wide range of polarization optics from a single supplier. The portfolio combines crystalline and polymer waveplates with solutions spanning UV through MWIR wavelengths, supporting applications ranging from life science and medical imaging to semiconductor manufacturing, laser processing, emerging quantum technologies, and more.

In addition to standard multiple-order, zero-order, and achromatic waveplates, the portfolio includes specialized products such as wide-angle, dual-wavelength, vacuum-compatible, high laser damage threshold (LDT), and quantum computing waveplates, many of which would typically require custom manufacturing. By making these products available off the shelf, Edmund Optics enables customers to purchase low quantities with fast delivery, helping accelerate prototyping and system development.

Customers also benefit from access to complementary optical and mechanical components available from the same supplier, simplifying procurement across the optical beam path. Together with fast shipping and 24/7 expert technical support, Edmund Optics® streamlines sourcing for both standard optical systems and demanding application-specific designs.

About Edmund Optics:

With over 80 years of experience, Edmund Optics is a trusted provider of high-quality optical components and solutions, serving industries like Life Sciences, Biomedical, Industrial Inspection, Semiconductor, and R&D. The company employs 1,300+ people across 19 global locations and continues to grow.

As a leading optics and photonics company, Edmund Optics provides two specialized solutions: a robust Marketplace with 34,000+ off-the-shelf products and Advanced Manufacturing, which focuses on custom and volume production of precision optical and imaging components.

Edmund Optics’ Marketplace is a one-stop shop for over 34,000 in-stock products from in-house manufacturing and 40+ top-tier brands, covering the entire beam path with fast, easy purchasing. For tailored solutions, Advanced Manufacturing offers custom design, first-article production, and scalable manufacturing — supported by four global design centres and nine specialized factories producing over 2 million components and 175,000+ assemblies annually.

Learn more at www.edmundoptics.com. 

 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号