您选择的产品已被添加至购物车

Edmund Optics® Expands Range of Handheld Infrared Viewers

Expanded product line offers wavelength, magnification, and sensitivity options for diverse laser applications

8/28/2025, Barrington, NJ USA —

 Edmund Optics® has expanded its range of Handheld Infrared (IR) Viewers, giving customers more choice and flexibility in how they approach IR laser visualization and system integration. The broader selection includes multiple magnification, wavelength and sensitivity configurations to address varied application needs.

Beyond the viewers themselves, Edmund Optics offers one of the industry’s most extensive portfolios of infrared optics and accessories, enabling customers to source complete solutions from a single partner. Options such as compatible C-mount lenses, IR filters, and camera adapters make it easy to tailor setups to evolving requirements, while extensive in-stock availability supports fast delivery and reduced downtime.

For organizations working across semiconductor, communications, biomedical, and industrial research, the expanded IR viewer family reinforces Edmund Optics’ role as a one-stop shop — combining product breadth and 24/7 application expertise. With the new additions, customers can align, monitor, and adapt their IR systems with greater confidence and efficiency.

About Edmund Optics®:

With over 80 years of experience, Edmund Optics is a trusted provider of high-quality optical components and solutions, serving industries like Life Sciences, Biomedical, Industrial Inspection, Semiconductor, and R&D. The company employs 1,300+ people across 19 global locations and continues to grow.

As a leading optics and photonics company, Edmund Optics provides two specialized solutions: a robust Marketplace with 34,000+ off-the-shelf products and Advanced Manufacturing, which focuses on custom and volume production of precision optical and imaging components.

Edmund Optics’ Marketplace is a one-stop shop for over 34,000 in-stock products from in-house manufacturing and 40+ top-tier brands, covering the entire beam path with fast, easy purchasing. For tailored solutions, Advanced Manufacturing offers custom design, first-article production, and scalable manufacturing — supported by four global design centres and nine specialized factories producing over 2 million components and 175,000+ assemblies annually.

Learn more at www.edmundoptics.com. 

Contact:

Agnes Huebscher, Senior Director, Global Corporate Marketing and Communications
[email protected]

 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号