您选择的产品已被添加至购物车

Edmund Optics Launches Ultraprecision Kinematic Mounts for Seamless System Integration and Repeatable Performance in Precision Applications

High-precision mounts now available alongside Edmund Optics' extensive range of optics – delivering complete, compatible, and ready-to-ship optical solutions from one trusted source.

10/29/2025, Barrington, NJ USA —

Edmund Optics® has expanded its optomechanics offering with the launch of Ultraprecision Kinematic Mounts, enabling customers to source both precision optics and precision mounts from a single, reliable partner.

The new mounts are engineered to align precisely with Edmund Optics’ existing optomechanics and components, ensuring immediate cross-family compatibility and effortless system integration. This allows engineers and research teams to build complete optical assemblies faster—without the alignment challenges that come from mixing suppliers.

By bringing mounts, optics, and support under one roof, Edmund Optics streamlines procurement and accelerates time to operation. With 34,000+ in-stock products, global 24/7 technical support, and decades of optical engineering expertise, the company delivers a unified ecosystem of components designed for performance, reliability, and ease of use.

For organizations developing high-performance or thermally sensitive optical systems, Edmund Optics now provides everything needed for precision alignment—from laser-grade optics to ultraprecision mounts—ready to ship and built to work together seamlessly.

About Edmund Optics®:

With over 80 years of experience, Edmund Optics is a trusted provider of high-quality optical components and solutions, serving industries like Life Sciences, Biomedical, Industrial Inspection, Semiconductor, and R&D. The company employs 1,300+ people across 19 global locations and continues to grow.

As a leading optics and photonics company, Edmund Optics provides two specialized solutions: a robust Marketplace with 34,000+ off-the-shelf products and Advanced Manufacturing, which focuses on custom and volume production of precision optical and imaging components.

Edmund Optics’ Marketplace is a one-stop shop for over 34,000 in-stock products from in-house manufacturing and 40+ top-tier brands, covering the entire beam path with fast, easy purchasing. For tailored solutions, Advanced Manufacturing offers custom design, first-article production, and scalable manufacturing — supported by four global design centres and nine specialized factories producing over 2 million components and 175,000+ assemblies annually.

Learn more at www.edmundoptics.eu 

Contact:

Agnes Huebscher, Senior Director, Global Corporate Marketing and Communications
[email protected]

 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号