您选择的产品已被添加至购物车

Edmund Optics Introduces Off-the-Shelf Extended Depth of Focus Metalenses for Laser Systems

Single-element, drop-in metalenses replace complex laser optics assemblies while maintaining precise focus over extended depth

4/7/2026, Barrington, NJ USA —
Edmund Optics®, a leading global provider of optical and imaging technology solutions, has announced the availability of off-the-shelf Extended Depth of Focus (EDOF) metalenses, making advanced meta-optics commercially accessible without the cost and delays of custom development. For the first time, engineers can source metalenses directly from the Edmund Optics Marketplace, enabling faster prototyping and accelerating the path from design to production.

By replacing more complex optical assemblies with a single flat component, EDOF metalenses can help reduce system size, complexity, and alignment requirements. The lenses maintain a controlled focal spot over an extended depth of focus, reducing sensitivity to positioning errors and minimizing the need for frequent refocusing. Designed for integration into select laser systems, including Ti:Sapphire, Yb-doped, and Nd:YAG lasers, the lenses are well suited for applications such as laser material processing, marking, and beam shaping, where consistency and performance are critical.

By bringing metalens technology into an accessible off-the-shelf offering, Edmund Optics enables organizations to move from concept to deployment faster while reducing risk and upfront investment. With immediate availability, engineering support, and access to a broad portfolio of 34,000+ complementary optical components, customers can now more efficiently design, prototype, and scale next-generation laser systems.

About Edmund Optics®:

With over 80 years of experience, Edmund Optics is a trusted provider of high-quality optical components and solutions, serving industries like Life Sciences, Biomedical, Industrial Inspection, Semiconductor, and R&D. The company employs 1,300+ people across 19 global locations and continues to grow.

As a leading optics and photonics company, Edmund Optics provides two specialized solutions: a robust Marketplace with 34,000+ off-the-shelf products and Advanced Manufacturing, which focuses on custom and volume production of precision optical and imaging components.

Edmund Optics’ Marketplace is a one-stop shop for over 34,000 in-stock products from in-house manufacturing and 40+ top-tier brands, covering the entire beam path with fast, easy purchasing. For tailored solutions, Advanced Manufacturing offers custom design, first-article production, and scalable manufacturing — supported by four global design centres and nine specialized factories producing over 2 million components and 175,000+ assemblies annually.

Learn more at www.edmundoptics.com.

Contact:

Agnes Huebscher
Senior Director Corporate Affairs, Communications and Industry Relations 
[email protected]
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号