您选择的产品已被添加至购物车

Edmund Optics® Continuous to Expand Its Off-the-Shelf Aperture Range for Precise Light Control

From laser beam shaping to advanced imaging setups, the right aperture can make a critical difference in optical system performance.

10/14/2026, Barrington, NJ USA —

Edmund Optics®, a leading global provider of optical and imaging technology solutions, offers optical designers and engineers easy access to one of the broadest selections of off-the-shelf apertures, making it straightforward to find the right solution for precise light control in imaging and laser systems. Options include adjustable iris diaphragms, precision pinholes and slits, aperture mounts, shutters, and more, readily available from stock for fast delivery.

To address diverse system requirements, apertures cover a wide range of sizes, materials, and mounting configurations. Specialized products extend from zero-aperture irises for complete light extinction to low-reflectance Acktar blackened pinholes with 99% absorption from EUV to SWIR and recently added chrome coated glass apertures. Also available are high-power laser apertures rated up to 130 MW/cm² and lockable iris diaphragms designed to resist shock and vibration in harsh environmental conditions. Manual and motorizable designs as well as C-, S-, and T-Mount solutions provide flexibility and facilitate system integration.

The broad portfolio enables customers to quickly select the right aperture for their application, while access to 34,000+ complementary optical and mechanical components from a single supplier simplifies the assembly of complete systems. Together with 24/7 live technical and application support, this extensive offering streamlines sourcing and keeps projects moving.

About Edmund Optics®

With over 80 years of experience, Edmund Optics® is a trusted provider of high-quality optical components and solutions, serving industries like Life Sciences, Biomedical, Industrial Inspection, Semiconductor, and R&D. The company employs 1,300+ people across 19 global locations and continues to grow.

As a leading optics and photonics company, Edmund Optics provides two specialized solutions: a robust Marketplace with 34,000+ off-the-shelf products and Advanced Manufacturing, which focuses on custom and volume production of precision optical and imaging components.

Edmund Optics’ Marketplace is a one-stop shop for over 34,000 in-stock products from in-house manufacturing and 40+ top-tier brands, covering the entire beam path with fast, easy purchasing. For tailored solutions, Advanced Manufacturing offers custom design, first-article production, and scalable manufacturing — supported by four global design centers and nine specialized factories producing over 2 million components and 175,000+ assemblies annually.

Learn more at www.edmundoptics.com.

 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号