Deviations in the surface form of an optical surface relative to its ideal shape at higher spatial frequencies than Zernike polynomial aberrations but lower frequencies than surface roughness. The mid-spatial frequency range is defined somewhat ambiguously as the region which causes optical blur or image degradation in optical systems. These errors must be controlled for during optical manufacturing, particularly when fabricating aspheric lenses.
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2023, 爱特蒙特光学(深圳)有限公司。— 广东省深圳市龙华工业东路利金城科技工业园3栋5楼 518109 - 粤ICP备2021068591号