The distance range through which a laser diode module can be focused to achieve an ideal spot size. Typically specified from the face of the module to past collimation. Although a laser diode module can be used at distances shorter than the minimum focusing range, it's spot size will be larger than the focused spot at this minimum distance. It is important to note that the focused spot size will increase with distance from the module. At long distances, the optimum focus condition is a collimated beam with minimum divergence.
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2023, 爱特蒙特光学(深圳)有限公司。— 广东省深圳市龙华工业东路利金城科技工业园3栋5楼 518109 - 粤ICP备2021068591号