The base of each ball bearing stage has 2 counterbored holes that accept socket head cap screws (SHCS). To gain access to the holes, move the mounting stage back and forth. It will help to use the side locking screw to hold the spring in place. The size of the screws depends on the stage; either #4, #6, or ¼. However, the length of the screws depends on the thickness of the adapter plate or the breadboard table (if connecting directly). We currently carry a line of breadboard adapter plates for such requirements with the S.H.C.S. included.
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2023, 爱特蒙特光学(深圳)有限公司。— 广东省深圳市龙华工业东路利金城科技工业园3栋5楼 518109 - 粤ICP备2021068591号