Holographic diffusers, a type of Holographic Optical Element (HOE), give a higher transmission of light than typical ground or opal glass diffusers. Because of their design, holographic diffusers also offer a more even distribution of light. They also give the added bonus of allowing the user to control the amount of diffusion by selecting the diffusion angle and aspect ratio. Holographic diffusers can increase transmission efficiency to greater than 90% from filament lamps, LEDs, arc lamps, and other sources. It is important to note that diffusing angles listed for these diffusers are for collimated light and angular divergence will vary for different incidence angles. Although they do offer better diffusion and control, they tend to be priced higher than typical ground or opal glass diffusers.
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2023, 爱特蒙特光学(深圳)有限公司。— 广东省深圳市龙华工业东路利金城科技工业园3栋5楼 518109 - 粤ICP备2021068591号