S&P polarization refers to the plane in which the electric field of a light wave is oscillating. S-Polarization is the plane of polarization perpendicular to the page (coming out of the monitor screen). P-polarization is the plane of polarization parallel to the page (in the plane of the monitor screen). See figure below:
When referring to polarization states, the p-polarization refers to the polarization plane parallel to the polarization axis of the polarizer being used ("p" is for "parallel"). The s-polarization refers to the polarization plane perpendicular to the polarization axis of the polarizer. A linear polarizer, by design, polarizes light in the p-polarization.
You offer a number of polarizers and retarders in both glass and film formats. Which one would be best for me?
The choice of polarizer substrate generally comes down to the optical needs of the system (i.e. weight and budget). In general, the glass filters tend to have higher quality polarizing characteristics. When surface accuracy is a concern (for instance in imaging applications), glass polarizers are preferable.
It is important to mount the polarizing filter, or any other filter, after the lens. Mounting the polarizer between the lens and the camera causes a change in the path difference between the sensor and the lens, and results in the image not being focused properly at the camera sensor plane. This effect holds true for all filters, such as ND filters, IR filters, etc. Our video lens specifications list the size of each lens' filter threading. Simply match the filter thread of the lens to the filter thread of our pre-mounted linear glass polarizing filters. The mounted filters have identical threads, so two can be used together to create a variable density effect.
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2023, 爱特蒙特光学(深圳)有限公司。— 广东省深圳市龙华工业东路利金城科技工业园3栋5楼 518109 - 粤ICP备2021068591号