The polarizing direction, also known as the polarization axis, runs parallel to the first mentioned dimension of the polarizing film. For example, a film with the dimension 500mm x 1000mm would have the polarizing direction running parallel to the 500mm side. Square polarizers have the polarizing direction indicated by a sticker on the protective film. In both cases the tolerance is +/- 2°.
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2023, 爱特蒙特光学(深圳)有限公司。— 广东省深圳市龙华工业东路利金城科技工业园3栋5楼 518109 - 粤ICP备2021068591号