A majority (but not all) of our first-surface mirrors are shipped with a protective plastic coating (a type of Molar® film overcoat) that protects the reflective surface. If the second surface is not ground, it looks like a second surface mirror when it is viewed from that side, but actually it is the bottom of the first surface coating reflecting through the glass. The plastic coating makes the top of the first surface look slightly dull and typically bluish in color as the mirror is tilted. The protective plastic coating can be removed by using Scotch® Tape or non-marring tweezers. Refer to the diagram below or view our video Removing Protective Plastic Coating for more information.
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2023, 爱特蒙特光学(深圳)有限公司。— 广东省深圳市龙华工业东路利金城科技工业园3栋5楼 518109 - 粤ICP备2021068591号