Strictly speaking, there are optical designs which enable fiber coupling without first collimating the output of the diode laser, but all of these designs suffer from massive astigmatism which can significantly reduce the efficacy of the fiber coupling. Having a collimated beam inside of the laser package allows for the addition of optical elements such as micro-optical isolators and bandpass filters.
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2023, 爱特蒙特光学(深圳)有限公司。— 广东省深圳市龙华工业东路利金城科技工业园3栋5楼 518109 - 粤ICP备2021068591号