The Modes or Mode Spacing of a laser beam refer to the quality of the laser beam. The Transverse Electromagnetic Mode (or TEM) describes the pattern that the laser spot makes. A TEM00 means a single laser spot (or beam cross-section) and it is typically used to specify how much of the laser output is in this mode. Due to its symmetrical beam intensity, this mode is typically selected. The total spectral bandwidth (sometimes referred to as the linewidth) is determined by multiplying the mode spacing value by (the number of modes minus one). For example, a He-Ne laser with a longitudinal mode spacing value of 730 MHz with 3 modes will have a total spectral bandwidth of 1.460 GHz. This defines the frequency range that most of the energy is distributed over.
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2023, 爱特蒙特光学(深圳)有限公司。— 广东省深圳市龙华工业东路利金城科技工业园3栋5楼 518109 - 粤ICP备2021068591号