High frequency illumination provides a flicker and ripple free output that assures image quality by maintaining constant frame to frame gray level. Fluorescent lights are the best example of high frequency illumination. When determining the correct illumination for one's camera setup, make sure the frequency of the illumination is higher than the frame rate of the camera. This will help to insure constant illumination and therefore the best image quality from frame to frame. Correspondingly, high frequency illumination helps reduce operator fatigue and eye strain when used over long durations.
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2023, 爱特蒙特光学(深圳)有限公司。— 广东省深圳市龙华工业东路利金城科技工业园3栋5楼 518109 - 粤ICP备2021068591号