As automated systems expand into a vast array of industries, imaging lenses are being introduced into new environments often experiencing harsh environments. A new generation of ruggedized lenses has been developed to protect from shock and vibration, water exposure, and temperature swings, to enable these automated systems.
This is Episode 9 in the Trending in Optics Video Series, in which one key trend in the optics and photonics industry is highlighted every several months. These conversations seek to shed some light on trending topics in optics and industry. Information on more technological and application advancements can be found at https://www.edmundoptics.com/knowledge-center/trending-in-optics/.
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2023, 爱特蒙特光学(深圳)有限公司。— 广东省深圳市龙华工业东路利金城科技工业园3栋5楼 518109 - 粤ICP备2021068591号