您选择的产品已被添加至购物车

How do I handle and clean my gratings?

Special care must be taken when handling and cleaning gratings. Handle only by the edges. Because the grooves are very tiny and delicate, the "drag method" for cleaning should not be used. Gratings have relatively soft coatings and are especially vulnerable to fingerprints and numerous aerosols, which can cause permanent damage.

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号