您选择的产品已被添加至购物车

Do you have lasers that can be used to cut or mark surfaces?

Edmund Optics does carry lasers that can be used to mark or cut select materials. The minimum power typically used with one of these lasers to cut or mark is more than ten Watts of power. At these kinds of output powers, safety is a major factor and must be taken into consideration.

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号