爱特蒙特光学(Edmund Optics®)使用自身以及第三方cookies来优化我们网站的技术服务功能. 了解我们如何使用cookies.

  • 我的帐户
  •   
资源 / 应用案例 / 激光 / Advantages of Using Beam Expanders
Advantages of Using Beam Expanders

Advantages of Using Beam Expanders

Focusing a laser beam down to a small spot is an integral part of many laser optical applications. While some applications benefit from large spot sizes, most require the smallest spot possible.

The spot size is usually defined as the radial distance from the center point of maximum irradiance to point where the intensity drops to 1/e2 of the initial value.

(1)$$ \definecolor{Diffraction}{RGB}{0, 0, 255} \definecolor{Aberration}{RGB}{255, 0, 0} \phi_{\text{Spot Size}} = \color{Diffraction} \phi_{\text{Diffraction}} \color{black} + \color{Aberration} \phi_{\text{Aberration}} \color{black} = \color{Diffraction} \frac{4 \lambda M^2 f}{\pi D} \color{black} + \color{Aberration} \frac{k D^3}{f^2} $$

λ:  Represents the wavelength
f:  Represents the focal length of your lens
D:  Represents the diameter of the input beam
k:  Represents the index of refraction of your lens
M2:  Represents the beam quality factor, this represents the degree of variation from an ideal Gaussian beam

The spot size is usually defined as the radial distance from the center point of maximum irradiance to point where the intensity drops to 1/e2 of the initial value.
Figure 1: The spot size is usually defined as the radial distance from the center point of maximum irradiance to point where the intensity drops to 1/e2 of the initial value.

Spot size is fundamentally determined by the combination of diffraction (red) and aberrations (blue). In this example we can assume that spherical aberration is the dominant aberration, and consider it the only type of aberration. For diffraction, we see that the shorter the focal length, the smaller the spot size. More importantly, the larger the input beam diameter, the smaller the spot size. This shows the advantage of using beam expanders in laser optical applications.

By expanding the beam within the system, the input beam diameter D is increased by a factor m, reducing the divergence by a factor m. When the beam is finally focused down to a small spot, this spot is a factor of m smaller than for the unexpanded beam for an ideal, diffraction limited spot. There is however a tradeoff with spherical aberration, which increases as the input beam diameter increases.

At small input beam diameters, the spot size is diffraction limited. As the input beam diameter increases, spherical aberration starts to dominate the spot size.
Figure 2: At small input beam diameters, the spot size is diffraction limited. As the input beam diameter increases, spherical aberration starts to dominate the spot size.
At short focal lengths, spherical aberrations dominate the spot size. At longer focal lengths, the spot size becomes diffraction limited.
Figure 3: At short focal lengths, spherical aberration dominates the spot size. At longer focal lengths, the spot becomes diffraction limited.
本内容对您是否有用?

View our selection of beam expanders to determine the best fit for your application.

Let Edmund Optics do the hard work for you! Determine the spot size of our lasers and laser diode modules by just inputting your working distance.

Knowing which beam expander is right for your application can greatly improve system efficiency. Learn about the different types and how to create your own custom design.

The most complete optics, imaging, and photonics video collection you’ll ever find. Browse 60+ video resources.

需要与爱特蒙特光学(Edmund Optics)联系?我们提供各种便捷、友好的服务以应对您的需求。

需要报价?

Edmund Optics Youku Edmund Optics Linkedin

×