To operate as efficiently as possible, the lenses require the incoming light to be circularly polarized. This requires extra care in the setup, and potentially additional polarization optics in the optical design. Also, the lenses function as a grating, and thus have significant chromatic aberration when used with broadband illumination. Care should be taken to limit the spectral bandwidth of the illumination for optimum results.
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2023, 爱特蒙特光学(深圳)有限公司。— 广东省深圳市龙华工业东路利金城科技工业园3栋5楼 518109 - 粤ICP备2021068591号