Lasers can induce photo-thermal and photo-chemical changes to retinal tissue to modify structures responsible for a specific vision impairment, like in LASIK.
Using IR Spectroscopy for Counterfeit Drug Detection
Infrared spectroscopy is used to detect harmful chemicals in counterfeit drugs making it critical to combat the opioid crisis, in the field or the lab.
How Trützschler and ITOS are Creating Cleaner Cotton
How Trützschler utilizes polarization to enable the more efficient processing of cotton providing a cleaner product and reducing rejected material in an effort to reduce waste and be more environmentally friendly.
The future depends on quickly and safely detecting elevated body temperatures that may indicate the presence of contagious diseases, such as COVID-19 (novel coronavirus).
Optics aid in the quick and accurate serological detection of antibodies to determine if a subject has an immune response to COVID-19, or the novel coronavirus.
The future depends on vision-guided technology that can safely sanitize hospitals, warehouses, and other locations to prevent the spread of contagious diseases, like COVID-19 (novel coronavirus).
Laser optics are critical for skin care procedures such as hair removal, acne and scar reduction, tattoo removal, sunspot removal, and skin revitalization.
Researchers from the University of Hawaii at Manoa use telecentric lenses and illuminators from Edmund Optics to advance our understanding of lung function.
Please select your shipping country to view the most accurate inventory information, and to determine the correct Edmund Optics sales office for your order.
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2023, 爱特蒙特光学(深圳)有限公司。— 广东省深圳市龙华工业东路利金城科技工业园3栋5楼 518109 - 粤ICP备2021068591号