eo_logo
  • 选择国家或地区
  • ,您好! 我的帐户
  • cart   
 

Nanostructured Nebular™ Technology for High-Power Laser Systems from Edmund Optics® Awarded Gold-Level Award

10/28/2020, Barrington, NJ USA   —

Edmund Optics® (EO) is proud to announce that Nebular™ Technology, a process for creating nanostructured anti-reflective laser optics with a high laser-induced damage threshold (LIDT), was awarded a Gold-Level 2020 Laser Focus World (LFW) Innovators Award in the optics category. Honorees of the LFW Innovators Awards are recognized for originality, answering an unmet need in the market, and positively impacting system integrators or end users.

Nebular™ Technology is an alternative to traditional thin-film anti-reflection (AR) coatings that is ideal for high-power laser applications. Subwavelength structures are etched into the surface of optical components rather than depositing coating layers. This leads to near-bulk laser LIDT and high broadband transmission. These surfaces achieve similar reflectivities as high-end, thin-film, anti-reflection coatings while operating over a significantly wider wavelength range.

No coating materials are added to the optical surfaces, which means the LIDT of surfaces featuring Nebular™ Technology can approach that of the uncoated substrate, which is significantly higher than the vast majority of conventional coatings. This is beneficial for high-power laser applications of all pulse durations ranging from continuous-wave (CW) to ultrafast lasers. Laser-induced damage in surfaces with Nebular™ Technology also does not propagate, unlike damage in thin films. This makes damage much more localized with a minimal impact on performance, avoiding the component failure experienced from damage propagation in thin-film coatings.

To learn more about Nebular™ Technology, please visit www.edmundoptics.com/nebular.

About EO:

Edmund Optics® (EO) is a leading global supplier of optics, imaging, and photonics technology that has served a variety of markets including Life Sciences, Biomedical, Industrial Inspection, Semiconductor, R&D, and Defense since 1942. EO designs and manufactures a wide array of optical components, multi-element lenses, imaging systems, and optomechanical equipment, while supporting OEM applications with volume production of stock and custom products. With locations in more than nine countries across the globe, EO employs just over 1,000 employees and continues to expand. Customers can purchase items by calling 1-800-363-1992, via the catalog, or on the website at www.edmundoptics.com.

认识设计、制造和交付爱特蒙特光学件的幕后团队。

我们在美洲、欧洲以及亚洲布局有15个区域办公室,您可在各个区域得到当地的支持以及世界级服务。

需要与爱特蒙特光学(Edmund Optics)联系?我们提供各种便捷、友好的服务以应对您的需求。

 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号
×