Need Help?

Our team is ready to assist you!


All About Aspheric Lenses

Anatomy of an Aspheric Lens | Benefits of an Aspheric Lens | Precision Glass Molding | Selecting the Right Aspheric Lens

ANATOMY OF AN ASPHERIC LENS

An aspheric lens, also referred to as an asphere, is a rotationally symmetric optic whose radius of curvature varies radially from its center. It improves image quality, reduces the number of required elements, and lowers costs in optical designs. From digital cameras and CD players to high-end microscope objectives and fluorescence microscopes, aspheric lenses are growing into every facet of the optics, imaging, and photonics industries due to the distinct advantages that they offer compared to traditional spherical optics.

Aspheric lenses have been traditionally defined with the surface profile (sag) given by Equation 1:

Equation 1(1)

Where

Z = sag of surface parallel to the optical axis
s = radial distance from the optical axis
C = curvature, inverse of radius
k = conic constant
A4, A6, A8 = 4th, 6th, 8th… order aspheric terms


As they have increased in popularity, there is now a more technically accurate way of describing the surface:

Equation 2(2)

Where

Cbfs = curvature of best fit sphere
ρ = radial distance from the optical axis
u = ρ/ρmax
Qmcon = orthonormal basis of asphere coefficients
am = normalization term

When the aspheric coefficients are equal to zero, the resulting aspheric surface is considered to be a conic. The following table shows how the actual conic surface generated depends on the magnitude and sign of the conic constant k.

Conic Constant Conic Surface
k = 0 Sphere
k > -1 Ellipse
k = -1 Parabola
k < -1 Hyperbola

The most unique geometric feature of aspheric lenses is that the radius of curvature changes with distance from the optical axis, unlike a sphere, which has a constant radius (Figure 1). This distinctive shape allows aspheric lenses to deliver improved optical performance compared to standard spherical surfaces.


Figure 1: Comparison of Spherical and Aspheric Surface Profiles [View Larger Image]

  1 , 2 , 3 | Next View All

相关产品

Optics Application Examples - 阅读我们为您制作并且广受欢迎的光学应用案例。学习探测器系统,选择合适的镜片,以及搭建投影系统。

Laser Spot Size Calculator - 根据使用者所提供的工作距离,使用EO技术工具来确定光斑尺寸。

EO 成像实验室 – 为您免费提供成像以及照明应用小窍门视频学习资料

Spotlight on EO - 技术图书馆中有哪些新内容?每个月我们都会有更新,请核对最新的技术更新。